SPI maximum operating speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI maximum operating speed

4,424 次查看
vijeshreddy
Contributor I

I am using phycore iMX6 module.

I have gone through the datasheet of imX6,  but could not find out the maximum operating speed of SPI module.

My requirement is to operate spi upto 80Mhz - is it possible?

标签 (1)
0 项奖励
回复
2 回复数

3,478 次查看
angelo_d
Senior Contributor I

Hi,

please correct me if i am wrong.

 

spectrum_0-1608242213852.png

 

Max speed for rx seems to be 18Mhz for slow pad group or 25 for fast pad group.

While if you only write on fifo, you should be able to reach up to 66Mhz.

Testings, using the "slow" pad group (18Mhz) seems i can
have proper values receivied only unitl 11Mhz,  that is not good ...

0 项奖励
回复

3,628 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you refer to Table 18-4 “System Clock Frequency Values” of the i.MX6DQ Reference Manual, you could verify the clock root option for SPI with a max frequency of 66.5 MHz.

You could also take a look at tables 21-6 and 8-4 of the same document for additional reference.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复