SPI for NOR Flash - Maximum addressable range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI for NOR Flash - Maximum addressable range

1,859件の閲覧回数
dvona
Contributor II

Greetings,

If one wanted to add flash memory to an i.MX6S with a SPI nor flash, what is the limiting factor for the maximum addressable memory?  I see references in the manual that state a 16k memory size size for SPI boot, and I also see a setting for 16-bit or 24-bit (but I'm not sure this refers to the address bits).

16kB.GIF.gif

24-bit.GIF.gif

ラベル(1)
0 件の賞賛
返信
1 返信

1,665件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Dan,

There is no limitation to the memory size on the SPI, of course the bigger the memory, the slower it'll become.

The table you are showing refers to the required memory for bootloader


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信