SPI for NOR Flash - Maximum addressable range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI for NOR Flash - Maximum addressable range

1,856 Views
dvona
Contributor II

Greetings,

If one wanted to add flash memory to an i.MX6S with a SPI nor flash, what is the limiting factor for the maximum addressable memory?  I see references in the manual that state a 16k memory size size for SPI boot, and I also see a setting for 16-bit or 24-bit (but I'm not sure this refers to the address bits).

16kB.GIF.gif

24-bit.GIF.gif

Labels (1)
0 Kudos
Reply
1 Reply

1,662 Views
SergioSolis
NXP Employee
NXP Employee

Hello Dan,

There is no limitation to the memory size on the SPI, of course the bigger the memory, the slower it'll become.

The table you are showing refers to the required memory for bootloader


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply