SPI driver for U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI driver for U-Boot

3,573 Views
AlexanderKeller
Contributor I

Hello,

does anybody know if there is a working SPI driver for U-Boot? We want to boot U-Boot from SPI flash and then also load the Linux Kernel from it.

Thanks in advance!

Labels (1)
0 Kudos
Reply
3 Replies

2,891 Views
WilliamHuang
NXP Employee
NXP Employee

Hi

    Would you please explain it in detail for the  u-boot-imx release and check the patch suggestion from Matthias Fuchs?

Thanks

BR

WilliamHuang

0 Kudos
Reply

2,891 Views
AlexanderKeller
Contributor I

Hi,

try the latest u-boot-imx release and check the patch suggestion from Matthias Fuchs. It works very well.

0 Kudos
Reply

2,891 Views
WilliamHuang
NXP Employee
NXP Employee
0 Kudos
Reply