SPI Slave Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Slave Mode

1,038件の閲覧回数
moose
Contributor IV

Is there a driver, example or a user space application that configure the SPI module within imx8mn in slave mode? Thx!

ラベル(1)
0 件の賞賛
返信
1 返信

1,021件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @moose ,

 

You can refer to arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts and arch/arm/boot/dts/imx6ul-14x14-evk-ecspi.dts.

Make sure not to use “cs-gpios” in dts. 

You should use should use “MX8MM_IOMUXC_ECSPI2_SS0_ECSPI2_SS0” instead of “MX8MM_IOMUXC_ECSPI2_SS0_GPIO5_IO13”.

 

Best regards.

 

Salas.

0 件の賞賛
返信