SPI-NOR programming with MFGTOOL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI-NOR programming with MFGTOOL

ソリューションへジャンプ
2,330件の閲覧回数
jparrish88
Contributor IV

Hello,

What is required to program SPI-NOR from the MFGTOOL on a custom board?

In other words what steps are necessary?

ラベル(1)
タグ(1)
1 解決策
1,990件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

please look at Linux Doc bundle

L3.0.35_4.1.0_LINUX_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf

Chapter 5 "Configuring the SPI NOR Flash Memory Technology Device (MTD) Driver",

then one needs to rebuild MFG Tool image (firmware file initramfs.cpio.gz.uboot)

check i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf

sect.3.9 "Building Manufacturing Firmware".

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,991件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

please look at Linux Doc bundle

L3.0.35_4.1.0_LINUX_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf

Chapter 5 "Configuring the SPI NOR Flash Memory Technology Device (MTD) Driver",

then one needs to rebuild MFG Tool image (firmware file initramfs.cpio.gz.uboot)

check i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf

sect.3.9 "Building Manufacturing Firmware".

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------