SPI-NOR programming with MFGTOOL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI-NOR programming with MFGTOOL

Jump to solution
2,320 Views
jparrish88
Contributor IV

Hello,

What is required to program SPI-NOR from the MFGTOOL on a custom board?

In other words what steps are necessary?

Labels (1)
Tags (1)
1 Solution
1,980 Views
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

please look at Linux Doc bundle

L3.0.35_4.1.0_LINUX_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf

Chapter 5 "Configuring the SPI NOR Flash Memory Technology Device (MTD) Driver",

then one needs to rebuild MFG Tool image (firmware file initramfs.cpio.gz.uboot)

check i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf

sect.3.9 "Building Manufacturing Firmware".

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,981 Views
igorpadykov
NXP Employee
NXP Employee

Hi jparrish88

please look at Linux Doc bundle

L3.0.35_4.1.0_LINUX_DOCS

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf

Chapter 5 "Configuring the SPI NOR Flash Memory Technology Device (MTD) Driver",

then one needs to rebuild MFG Tool image (firmware file initramfs.cpio.gz.uboot)

check i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf

sect.3.9 "Building Manufacturing Firmware".

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------