SPI Chip Select Behavior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Chip Select Behavior

2,105件の閲覧回数
moose
Contributor IV

Shouldn't chip select signal stay asserted for the entire transmission of a multi-byte frame? When I send an 8-byte frame, I see the CS go high after every byte, as shown below. Is this expected? Is there a way to configure it to stay asserted throughout the frame? I tried both spidev_test and spi-pip and experienced the same behavior. Below are the user space commands I tried. Any input? Thx!

`spidev_test -D /dev/spidev1.0 -v -p "\x55\x55\x55\x55\x00\x00\xff\xff"`

`printf '\x55\x55\x55\x55\x00\x00\xff\xff' | spi-pipe -d /dev/spidev1.0 --blocksize=8 | hexdump -C`

moose_0-1706903358685.png

CH1 (yellow) = SPI_CLK

CH2 (blue) = SPI_nCS

 

ラベル(1)
0 件の賞賛
返信
1 返信

2,059件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @moose, 

Thank you for contacting NXP Support.

No, that is not the expected behavior. I have tested on my side using the BSP version 6.1.55 and here are my results.

brian14_0-1707240417612.png

Could you please tell me your BSP, your processor and if you are using an EVK or custom board?

0 件の賞賛
返信