SPI 9-bit mode U-boot for imx6sl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI 9-bit mode U-boot for imx6sl

1,047 Views
nigelevans
Contributor III

Hi,

I am trying to initialize an SPI device from u-boot.

I have setup ecspi3 pin mux pad definitions and initial directions and states.

What I am looking for is an example of how to perform 9-bit writes to a device from within u-boot. Does anyone have an example or can someone point me in the right direction please?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

908 Views
Yuri
NXP Employee
NXP Employee

Hello

   Please refer to sections 19.5 (Initialization) and 19.6 (Applications) of the i.MX6 SL Reference 
Manual (IMX6SLRM, Rev. 2, 06/2015)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply