SNVS security state transition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS security state transition

1,466件の閲覧回数
yilingxu
Contributor III

On Imx6q board, I see NSVS has four security modes: Trusted, Secure, Non-secure, Fail. And I see the security state transitions as follow:

647150211.jpg

I want to ask, what's mean of reset of SOC? RePower the board can be considered as "reset of SOC"? Or press the SW2-Board Reset Button can be considered as "reset of SOC"?

1449034969.jpg

Thanks,

Yiling Xu

ラベル(1)
0 件の賞賛
返信
1 返信

1,388件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You some comments directly via e-mail.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信