SNVS LPGPR write times

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SNVS LPGPR write times

ソリューションへジャンプ
2,844件の閲覧回数
xiongweihuang
Contributor III

Hello all

From https://community.freescale.com/docs/DOC-93964

SNVS LPGPR is used for power up check boot mode

And in this case . it will not be write over than 100k times

my concern

for a long time product life

In some other special use case . if we dairy write it over 100 times a day ,over 10 years  ,is it be strong enough ?

How much times can we write on this register ?

Thanks and regards 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,186件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

SNVS LPGPR is basically SRAM cell, not flash technology,

so number of programming times ("write over") is unlimited.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,187件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

SNVS LPGPR is basically SRAM cell, not flash technology,

so number of programming times ("write over") is unlimited.

0 件の賞賛
返信
2,186件の閲覧回数
xiongweihuang
Contributor III

Thanks

0 件の賞賛
返信