SNVS LPGPR write times

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SNVS LPGPR write times

Jump to solution
2,842 Views
xiongweihuang
Contributor III

Hello all

From https://community.freescale.com/docs/DOC-93964

SNVS LPGPR is used for power up check boot mode

And in this case . it will not be write over than 100k times

my concern

for a long time product life

In some other special use case . if we dairy write it over 100 times a day ,over 10 years  ,is it be strong enough ?

How much times can we write on this register ?

Thanks and regards 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,184 Views
igorpadykov
NXP Employee
NXP Employee

Hi

SNVS LPGPR is basically SRAM cell, not flash technology,

so number of programming times ("write over") is unlimited.

View solution in original post

0 Kudos
Reply
2 Replies
2,185 Views
igorpadykov
NXP Employee
NXP Employee

Hi

SNVS LPGPR is basically SRAM cell, not flash technology,

so number of programming times ("write over") is unlimited.

0 Kudos
Reply
2,184 Views
xiongweihuang
Contributor III

Thanks

0 Kudos
Reply