SLC NAND Flash Hardware Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SLC NAND Flash Hardware Configuration

ソリューションへジャンプ
2,171件の閲覧回数
atillametetured
Contributor V

Greetings,

Can someone please tell me how to connect a NAND Flash to i.MX6Q processor HW-wise such as which pins are

used for the mentioned NAND Flahs Interface or direct me to a document where regarded information shall be found.

Is there a related sample design anyone knows. Variscite has usen them but their schematics are not open source

and since Sabre uses NOR Flash I believe that wont be any good to me.

Thanks in advance,

Mete

ラベル(2)
0 件の賞賛
返信
1 解決策
2,093件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6 SABRE for Automotive board uses the NAND Flash, please refer to its schematic, available for download on the NXP web site (check the "Schematics" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,094件の閲覧回数
art
NXP Employee
NXP Employee

The i.MX6 SABRE for Automotive board uses the NAND Flash, please refer to its schematic, available for download on the NXP web site (check the "Schematics" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,093件の閲覧回数
atillametetured
Contributor V

Hello Artur,

I surely have missed that because I checked the Sabre2.

Thanks a lot,

Mete

0 件の賞賛
返信