SIM interface iMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SIM interface iMX6UL

2,018件の閲覧回数
riteshpatel
Contributor II

Hi,

I am bit confuse about SIM interface on iMX6UL. 

As per technical reference manual page # 2799, "The SIM module has one port that can be used to interface with the various cards."  But block diagram shows two port, 0 & 1.

pastedImage_1.png

Referred i.MX6UL pin muxing, Found that there are four ports.

SIM1.Port0,

SIM1.Port1,

SIM2.Port0,

SIM2.Port1.

Will appreciate any help or clarification for understanding above with reference if any.

Can you please let me know on which two SIM ports i can connect smart card? As datasheet shows upto 2 SIM interface support.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,692件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Each SIM module can be connected to two separate devices via Port0 and Port1,

however communication to two devices from a single SIM module is alternate and
can not provide simultaneous communication. Please refer to SIM Setup Register

how to configure ports.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信