SGTL5000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000

2,509件の閲覧回数
rizwan_s
Contributor II

Hi

I am working on imx6 solo custom board.presently working on audio sgtl5000 .

I have changed the dts file for iomux settings and sgtl5000 related settings.

Sgtl5000 is registered ,i can confirm it through aplay -l command. But when i play the file sound does not come.only some junk sound comes always when i connect the headphone.

Please suggest what is the issue,is am missing configuartion

Thanks and Regards

Rizwan Syed

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

2,168件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

one can test with oscilloscope mclk sgtl5000 signal.

Please check its settings (CLKO1 pad) using BD boards configurations,

for example imx6qdl-sabrelite.dtsi

linux-imx6/imx6qdl-sabrelite.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

Schematic with sgtl5000 connections can be found on

i.MX6 ARM Development Board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,168件の閲覧回数
rizwan_s
Contributor II

Hi Igor,

Thanks for your reply.

I have checked the clock ,it is 24 MHz and MX6QDL_PAD_GPIO_0__CCM_CLKO1    0x000b0.

Thanks and Regards

Rizwan Syed

0 件の賞賛
返信

2,168件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

what about bit clock and frame sygnal. What procesor used in the case.

Had you tried with baremetal SDK:

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor

0 件の賞賛
返信