SGTL5000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000

2,519 Views
rizwan_s
Contributor II

Hi

I am working on imx6 solo custom board.presently working on audio sgtl5000 .

I have changed the dts file for iomux settings and sgtl5000 related settings.

Sgtl5000 is registered ,i can confirm it through aplay -l command. But when i play the file sound does not come.only some junk sound comes always when i connect the headphone.

Please suggest what is the issue,is am missing configuartion

Thanks and Regards

Rizwan Syed

Labels (4)
0 Kudos
Reply
3 Replies

2,178 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

one can test with oscilloscope mclk sgtl5000 signal.

Please check its settings (CLKO1 pad) using BD boards configurations,

for example imx6qdl-sabrelite.dtsi

linux-imx6/imx6qdl-sabrelite.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

Schematic with sgtl5000 connections can be found on

i.MX6 ARM Development Board 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,178 Views
rizwan_s
Contributor II

Hi Igor,

Thanks for your reply.

I have checked the clock ,it is 24 MHz and MX6QDL_PAD_GPIO_0__CCM_CLKO1    0x000b0.

Thanks and Regards

Rizwan Syed

0 Kudos
Reply

2,178 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

what about bit clock and frame sygnal. What procesor used in the case.

Had you tried with baremetal SDK:

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Best regards
igor

0 Kudos
Reply