SGTL5000 support on Android 7.1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 support on Android 7.1.2

2,272 Views
aravinthkumarja
Senior Contributor II

Hi All,

I'm using Android 7.1.2 on imx6q platform. Our Audio codec is sgtl5000, When board boots it is detecting on kernel level. I need to integrate on Android HAL layer.

So Can you provide "config_sgtl5000.h" and porting patches for Android 7.1.2.?

Regards,

Aravinth

Labels (3)
0 Kudos
Reply
3 Replies

1,951 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

nxp reference boards do no have sgtl5000, please check BD, which boards have

that codec, android releases

Android Nougat 7.1.1 release for i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,951 Views
aravinthkumarja
Senior Contributor II

Hi igor.

I didn't get anything about sgtl5000 on your mentioned link.

Please give a valid response.

Regards,

Aravinth

0 Kudos
Reply

1,951 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aravinth

please check suggested link, Boundary Devices android releases

support sgtl5000. NXP bsps do not support it.

Best regards
igor

0 Kudos
Reply