SELinux Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SELinux Support

2,760 Views
vishakh
Contributor III

Hi,

Is i.MX6X support is provided in SELinux and  SELinux Android?

If yes, what are SELinux and SELinux Andriod versions available with the i.MX6X support?

Thanks and Regards,

Vishakh

0 Kudos
Reply
3 Replies

2,544 Views
gary_bisson
Senior Contributor III

Hi Vishakh,

Yes NXP Android releases support SELinux since KitKat 4.4.x.

You can find more on the subject here:

https://boundarydevices.com/android-security-part-3-security-enhanced-linux-in-android/ 

Regards,

Gary

2,544 Views
vishakh
Contributor III

Hi gary_bisson‌,

Thank you for the prompt reply.

Would you please let me know what is the SELinux kernel version with i.MX6X support?

With Regards,

Vishakh

0 Kudos
Reply

2,544 Views
gary_bisson
Senior Contributor III

Hi Vishakh,

It depends on the Android version you want to use. For instance, Marshmallow release is using kernel 4.1.15. You can have a look at the git repo to see all the Android releases kernel version:

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Regards,

Gary

0 Kudos
Reply