Hi,My Bsp is imx6q_L3_14_52, and run the command:
./mxc_vpu_test.out -L "-f 0 -w 720 -h 480"
[INFO] VPU test program built on Oct 13 2016 11:33:55
[INFO] Product Info: i.MX6Q/D/S
[INFO] VPU firmware version: 3.1.1_r46070
[INFO] VPU library version: 5.4.32
[INFO] Format: STD_MPEG4
[INFO] MPEG4 class: MPEG4
[INFO] Capture/Encode fps will be 30
[INFO] ringBufferEnable 0, chromaInterleave 1, mapType 0, linear2TiledEnable 0
[INFO][ 405.662937] mxc v4l2 capture:mxc v4l2 s param test !!!!!!!!
sensor chip is adv7180_decoder
[INFO] sensor frame size is 720x480
[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0
[INFO] Mpeg4 Profile: 0 Level: 7 Interlaced: 0
[INFO] Aspect Ratio Table index: 1
[INFO] Decoder: width = 720, height = 480, frameRateRes = 30, frameRateDiv = 4294967295, count = 4
[INFO] CROP left/top/right/bottom 0 0 0 0
[INFO] v4l output to /dev/video17
[INFO] Display to 720 480, top offset 0, left offset 0
[INFO] Display: NV12
[INFO] Display fps will be 30
But the display video is rolling on LCD,Why ? How to solve it ? thanks!
did you use adv7180? if yes, I think you should use mxc_v4l2_tvin.out.
and I'm not sure what mode do you use, one can refer this thread too.
Hi Joan,
thanks your reply, i modify the cam->crop_current.top, and call ioctl VIDIOC_G_STD , now I can get the initial value of cam->crop_current.top , and cam->crop_current.top is set value, the display keep scrolling down slower, how can i solve it ? thanks.