SDRAM on IMXRT1176 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDRAM on IMXRT1176 EVK

跳至解决方案
1,054 次查看
smartpavan333
Contributor I

Hi,

I am using IMXRT1176-EVK-Board.

I am taking SDK example of sdjpeg.

In EVK board two SDRAM's but  we want to run the sdjpeg example run on single SDRAM.

0x00-SDRAM CS0.
0xFF - Full configuration. Must configure all fields.

Where should I modify? 

Note: I am Using IAR IDE.

Can you help me this issue?

0 项奖励
回复
1 解答
1,041 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You might want to limit the SEMC size for SDRAM to only be only 256Mb so only one memory is used. This can be done on MIMXRT11##xxxxx_sdram.icf file.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,042 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

You might want to limit the SEMC size for SDRAM to only be only 256Mb so only one memory is used. This can be done on MIMXRT11##xxxxx_sdram.icf file.

Best regards,
Omar

0 项奖励
回复