SDRAM CLK Assignment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,141件の閲覧回数
mrudangshelat
Contributor IV

Hi, I was referring SABRESDB (SPF-27516_C5) for my ongoing design. Is there any specific reason to assign SDCLK1 to Lower DATABUS DRAM_D[31:0] and SDCLK0 to Higher DATABUS DRAM_D[63:32]? I would like to know because generally I have seen SDCLK1 to higher DATABUS DRAM_D[63:32 and SDCLK0 to lower DATABUS DRAM_D[31:0]. Regards, Mrudang

ラベル(2)
1 解決策
2,027件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

there is no special reason as both signals are identical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,028件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

there is no special reason as both signals are identical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,027件の閲覧回数
mrudangshelat
Contributor IV

Hi Igor,

If I use CLK1 instead of CLK 0 for lower data-bus D[15:0], A[15:0] and other controller will be having interfaced on CS0, CKE0 and ODT0.

  1. Does it effect power consumption of DDR SDRAM?
  2. Do iMX6 has Single or Dual DDR Controller/channel?

Regards,

Mrudang

0 件の賞賛
返信