SDMA external request and EIM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDMA external request and EIM

2,478 次查看
sharpjison
Contributor II

Hello NXP:

         My project is to use SDMA to transfer FPGA data via EIM interface.

         I want to use SDMA external request to stop the action, when the FPGA data is not ready.

         How can I use external SDMA request pins to start a logic channel transfer over the EIM interface ?

 

         My EIM config  :

                    Multiplexed  Address/Data mode  16Bit

                    Asynchronous Read Access

         

The code is as floows:

//#include <linux/config.h>
#include <linux/moduleparam.h>
#include <linux/module.h>
#include <linux/version.h>
#include <linux/types.h>
#include <linux/errno.h>
#include <linux/kernel.h>
#include <linux/init.h>
 
#include <linux/timer.h>
#include <linux/sched.h>
#include <linux/interrupt.h>
#include <linux/pm.h>
#include <linux/spinlock.h>
#include <linux/delay.h>
 
#include <linux/device.h>
#include <linux/dma-mapping.h>
 
#include <linux/io.h>
 
#include <linux/slab.h>
#include <linux/mman.h>
#include <linux/kthread.h>
#include <linux/dmaengine.h>
#include <linux/platform_data/dma-imx.h>
#include <linux/platform_data/dma-imx-sdma.h>
 
#include <linux/workqueue.h>  
 
#define DMA_SOURCE_ADDR          0x08000000
 
#define DMA_START_ADDR           0x30000000  
#define DMA_DATA_LENGTH          0x00020000  
 
#define BUFF_START_ADDR          0x40000000
#define BUFF_DATA_LENGTH         0x00020000
 
struct timespec ts_start;
struct timespec ts_end  ;
 
struct timeval  tv_start;
struct timeval  tv_end  ;
 
int cnt;
 
struct thread_data {
    int nr;
    pid_t pid;
    char * name;
};
 
struct dma_transfer {
    struct dma_chan *ch;
    struct dma_slave_config dma_m2m_config;
    struct dma_async_tx_descriptor *dma_m2m_desc;
    struct completion dma_m2m_ok;
    unsigned int   phys_from;
    unsigned int   phys_to;
};
 
static int  dmatest_work(void *data);
static void dma_memcpy_callback_from_fpga(void *data);
static int  dma_mem_transfer_to_store_buffer(void) ;
 
static unsigned int  data_addr ;
static unsigned int  buff_addr ;
static struct dma_transfer dma_data   ;  
static struct dma_transfer dma_buffer ;
 
static bool dma_m2m_filter (struct dma_chan *chan, void *param)
{
    if (!imx_dma_is_general_purpose(chan))
        return false;
    chan->private = param;
    return true;
}
 
static void dma_memcpy_callback_to_buffer(void *data)
{
static void dma_to_store_buffer(void)
{
    struct dma_transfer* dma = &dma_buffer ;
 
    dma->dma_m2m_config.direction = DMA_MEM_TO_MEM;
    dma->dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
    dmaengine_slave_config(dma->ch, &dma->dma_m2m_config);
    dma->dma_m2m_desc = dma->ch->device->device_prep_dma_memcpy(dma->ch,
                                        dma->phys_to, dma->phys_from,
                                        0x00020000, 0);
    dma->dma_m2m_desc->callback = dma_memcpy_callback_to_buffer;
    dmaengine_submit(dma->dma_m2m_desc);
    dma_async_issue_pending (dma->ch);
}
 
// dma to buffer channel init
static int dma_mem_transfer_to_store_buffer(void)
{
    struct dma_transfer* dma = &dma_buffer ;
 
    dma_cap_mask_t dma_m2m_mask;
    struct imx_dma_data m2m_dma_data = {0};
 
    dma_cap_zero (dma_m2m_mask);
    dma_cap_set (DMA_SLAVE, dma_m2m_mask);
    m2m_dma_data.peripheral_type = IMX_DMATYPE_MEMORY;
    m2m_dma_data.priority = DMA_PRIO_HIGH;
 
    memset(dma, 0, sizeof(struct dma_transfer));
    dma->phys_from   =  DMA_START_ADDR   ;
    dma->phys_to     =  BUFF_START_ADDR  ;
 
    dma->ch = dma_request_channel(dma_m2m_mask, dma_m2m_filter, &m2m_dma_data);
    if (!dma->ch) {
        printk(KERN_ERR "Could not get DMA with dma_request_channel()\n");
        return -ENOMEM;
    }
     
    return 0;
}
 
/*
 * The callback gets called by the DMA interrupt handler after
 * the transfer is complete.
 */
static void dma_memcpy_callback_from_fpga(void *data)
{
    dma_to_store_buffer() ;
    
    dma_data.dma_m2m_config.direction = DMA_MEM_TO_MEM;
    dma_data.dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
    dmaengine_slave_config(dma_data.ch, &dma_data.dma_m2m_config);
    dma_data.dma_m2m_desc = dma_data.ch->device->device_prep_dma_memcpy(dma_data.ch,
                                        dma_data.phys_to, dma_data.phys_from,
                                        0x00020000, 0);
    dma_data.dma_m2m_desc->callback = dma_memcpy_callback_from_fpga;
    dmaengine_submit(dma_data.dma_m2m_desc);
    dma_async_issue_pending (dma_data.ch);
     
    return ;
}
 
static int dma_mem_transfer_from_fpga (void)
{
    struct dma_transfer* dma = &dma_data ;
 
    dma_cap_mask_t dma_m2m_mask;
    struct imx_dma_data m2m_dma_data = {0};
 
    dma_cap_zero (dma_m2m_mask);
    dma_cap_set (DMA_SLAVE, dma_m2m_mask);
    m2m_dma_data.peripheral_type = IMX_DMATYPE_MEMORY;
    m2m_dma_data.priority = DMA_PRIO_HIGH;
 
    memset(&dma_data, 0, sizeof(struct dma_transfer));
    dma->phys_from    = DMA_SOURCE_ADDR;
    dma->phys_to    = DMA_START_ADDR ;
     
    dma->ch = dma_request_channel(dma_m2m_mask, dma_m2m_filter, &m2m_dma_data);
    if (!dma->ch) {
        printk(KERN_ERR "Could not get DMA with dma_request_channel()\n");
        return -ENOMEM;
    }
 
    dma->dma_m2m_config.direction = DMA_MEM_TO_MEM;
    dma->dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_4_BYTES;
    dmaengine_slave_config(dma->ch, &dma->dma_m2m_config);
    dma->dma_m2m_desc = dma->ch->device->device_prep_dma_memcpy(dma->ch,
                                        dma->phys_to, dma->phys_from,
                                        0x00020000,0);
    dma->dma_m2m_desc->callback = dma_memcpy_callback_from_fpga;
    dmaengine_submit(dma->dma_m2m_desc);
    dma_async_issue_pending (dma->ch);
 
    do_gettimeofday (&tv_start);
    ts_start = current_kernel_time ();
 
    return 0;
}
 
static int   dmatest_work (void *data)
{
    dma_mem_transfer_from_fpga();
    // DMA data to store buffer
    dma_mem_transfer_to_store_buffer() ;
 
    return 0;
 
}
 
static char *name = "dmatest";
 
static int __init dmatest_init(void)
{
    struct thread_data * thread;
    /* Schedule multiple concurrent dma tests */
    thread = kmalloc(sizeof(struct thread_data), GFP_KERNEL);
    if (!thread) {
        goto free_threads;
    }
 
    memset(thread, 0, sizeof(struct thread_data));
    thread->nr = 1;
    thread->name = name;
 
    /* Schedule the test thread */
    kthread_run (dmatest_work, thread, thread->name);
 
    request_mem_region(DMA_START_ADDR, DMA_DATA_LENGTH, "dma_data");
    data_addr = (unsigned int )ioremap(DMA_START_ADDR, DMA_DATA_LENGTH);
 
    request_mem_region(BUFF_START_ADDR, BUFF_DATA_LENGTH , "buffer_data");
    buff_addr = (unsigned int )ioremap( BUFF_START_ADDR , BUFF_DATA_LENGTH );
 
    printk("<0>dma module is running !\n");
    return 0;
 
free_threads:
    kfree(thread);
 
    return -ENOMEM;
}
 
static void __exit dmatest_exit(void)
{
    return;
}
 
MODULE_LICENSE("Dual BSD/GPL");
module_init(dmatest_init);
module_exit(dmatest_exit);

标签 (3)
0 项奖励
回复
4 回复数

2,044 次查看
jial2012
Contributor II

Hi Sharp:

     did you solved your question? I have the same case about how to triggle the external SDMA request pins. if you solved your  problem , please guide something help for me! thanks!

   Best regards

      lingjia

0 项奖励
回复

2,044 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

I am afraid external SDMA request is not supported BSPs, however

one can try to add it using existing uart example (it uses fifo level request signal)

please look at description of IOMUXC_GPR0[7]:
iomux.sdma_ext_events[1] - External DMA Request via DISP0_DAT17 or GPIO_18
and sect.3.3 SDMA event mapping Event N14 i.MX6DQ Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
By detecting a external DMA request signal the SDMA can be triggered to perform the
associated channel task.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,044 次查看
sharpjison
Contributor II

Hi igorpadykov:

Thanks for your reply.

The infomation about IOMUXC_GPR0[7] and iomux.sdma_ext_events[1] is a liite brief in the datasheet .

Can you give me a demo or a guide to let me know how to config ?

  

Best regades.

Have a nice day !

0 项奖励
回复

2,044 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

unfortunately such demo is not available.

Best regards
igor

0 项奖励
回复