SDK2.2_iMX6UL_WIN for new create project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK2.2_iMX6UL_WIN for new create project

1,920 次查看
kyleyang
Contributor IV

Hi sirs,

I had download the SDK2.2_iMX6UL_WIN and try to create a new stand alone freeRTOS project code.

I try to use "KSDK-Project-Generator" tool to create or clone a project code, but not works.

Is there any recommend method for me to solve this issue?

thanks.

标签 (2)
标记 (2)
0 项奖励
回复
2 回复数

1,679 次查看
art
NXP Employee
NXP Employee

Please refer to the attached document. It is also included in the SDK package.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,679 次查看
kyleyang
Contributor IV

Hi Artur

Thanks.

I had check that before, but did not match what I need.

I want to new create a stand alone project code, is there any way to achieve?

0 项奖励
回复