SDK failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK failure

3,750 Views
cowles
Contributor I
Using MCUXpresso IDE v 11.8.0, attempt to install the SDK for board "evkbimxrt1050" always results 
in the error:
"An error occurred while installing the items
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Install, operand=null -->
[R]org.eclipse.jdt.core.manipulation 1.17.0.v20221026-1918, action=org.eclipse.equinox.internal.p2.touchpoint.eclipse.actions.InstallBundleAction).
The artifact file for osgi.bundle,org.eclipse.jdt.core.manipulation,1.17.0.v20221026-1918 was not found."

This also occurred with older versions of MCUXpresso! Will anyone ever fix this?
0 Kudos
Reply
5 Replies

2,741 Views
dstevens
Contributor II

Seems I accidentally deleted my original reply. See below:

The error you describe is sometimes shown by Eclipse when it is trying to write a file without permission. Some SDK installations will try to modify Eclipse plugins etc. and trigger this.

The core problem that leads to this is NXP installing MCUXpresso into `/opt` instead of the users home folder (like TI do with CCS).

As a workaround, you can try running MCUXpresso as root just to install the SDK. I've had success doing this or plugin installation when MCUXpresso was giving the same error.

And to the NXP team, please change the install location under Linux to the user's home folder. This will prevent this and many other problems (such as application note sample code not working because it expects the source files to be under the same parent folder as the IDE)

0 Kudos
Reply

3,577 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @cowles ,

What's your OS and how do you download the SDK?

 

Regards,

Jing

0 Kudos
Reply

3,525 Views
cowles
Contributor I

I am using Debian versions 11 and 12 on two different machines. The problem comes when you

"download and install SDKs" at the mcuxpresso welcome screen. Separately downloading an SDK

and passing it to mcuxpresso does work. I have used several versions of mcuxpresso with several

different EVK's, and they all do the same thing. Why invite people to use it if it doesn't work?

Chris

0 Kudos
Reply

3,498 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @cowles ,

I'll report this issue to software team. Please download SDK from mcuxpresso.nxp.com currently.

 

Regards,

Jing

0 Kudos
Reply

3,344 Views
stefanct
Contributor IV

Are there any news about this? I am a first-time user of mcuxpresso and neither the in-built download nor the manual install works for me.

Dropping the .zip downloaded from the SDK builder into the "Installed SDKs" view results in the following dialog with an deactivated OK button (presumably because the .manifest field is left empty... because I don't know where it should come from):

stefanct_0-1695656587277.png

 

Using the alternative via "Import archive..." results in

stefanct_2-1695657123779.png

 

All of this with MCUXpresso IDE v11.8.0 [Build 1165] [2023-07-26] on Debian stable (12).

0 Kudos
Reply