SDK - Enabling interrupts under u-boot control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK - Enabling interrupts under u-boot control

1,471件の閲覧回数
dancer
Contributor I

Hi all,

the current platform SDK (version 1.1.0) provides some examples which are using interrupts.

The examples which are not using interrupts can be successfully loaded and started with u-boot commands.
If you try to to start an example (under u-boot control) which uses interrupts the system will hang.

Attached you will find a patch series which solves this issue on my side. (the patch is for RFC and contains only one example: epit)

BTW, for tests I use a Sabre Lite development board (i.MX6 quad core).

Original Attachment has been moved to: 0002-SDK-fix-linker-script-for-VBAR-support.patch.zip

Original Attachment has been moved to: 0003-SDK-epit-test-fix-interrupt-support-by-using-VBAR.patch.zip

Original Attachment has been moved to: 0001-Cortex-A9-add-get-set-_vbar-helper-functions.patch.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,380件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ralf

thanks for sharing codes and experience.

I think is will be useful for board bring-up purposes.

Best regards

chip

0 件の賞賛
返信