SDIO interface in I.MX508 maximum speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDIO interface in I.MX508 maximum speed

978 次查看
lyfsci
Contributor III

Hi Experts,

Does I.MX50 supports SDIO host interface as well ? I could observe that it has MMC/SD interface..

What is the maximum operating speed in which it operate ?

标签 (1)
0 项奖励
回复
1 回复

857 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lyf

yes, i.MX50 eSDHC module supports SDIO,

52MHz max. frequency is given by

IMX50CEC Table 51. SD/eMMC4.3 Interface Timing Specification

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复