SDIO command timeout issue with SD8787 wifi chipset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDIO command timeout issue with SD8787 wifi chipset

34,708 次查看
krishnanp
Contributor III

Platform: sabre-lite imx6 Q board

Kernel: 3.0.35

Wifi chipset: Marvell SD8787 based wifi module

wifi driver : mwifiex

We are facing an issue in Wi-Fi bring-up  on 3.0.35  kernel.  The Wi-Fi module connected to sabre-lite board through SDIO interface.

The driver is able to load the firmware. But if  we try to a data transfer the driver crashes with following message.

root@freescale /$ dhclient mlan0
Internet Systems Consortium DHCP Client V3.0.3b1
Copyright 2004-2005 Internet Systems Consortium.

Listening on Socket/eth0
Sending on   Socket/eth0
Listening on Socket/mlan0
Sending on   Socket/mlan0
Sending on   Socket/fallback
DHCPDISCOVER on mlan0 to 255.255.255.255 port 67 interval 6
DHCPDISCOVER on eth0 to 255.255.255.255 port 67 interval 4
DHCPDISCOVER on mlan0 to 255.255.255.255 port 67 interval 9
DHCPDISCOVER on eth0 to 255.255.255.255 port 67 interval 8
mwifiex_sdio mmc1:0001:1: mwifiex_cmd_timeout_func: Timeout cmd id (97.892473) = 0xce, act = 0x1c8c
mwifiex_sdio mmc1:0001:1: num_data_h2c_failure = 0
mwifiex_sdio mmc1:0001:1: num_cmd_h2c_failure = 0
mwifiex_sdio mmc1:0001:1: num_cmd_timeout = 1
mwifiex_sdio mmc1:0001:1: num_tx_timeout = 0
mwifiex_sdio mmc1:0001:1: last_cmd_index = 3
mwifiex_sdio mmc1:0001:1: last_cmd_resp_index = 2
mwifiex_sdio mmc1:0001:1: last_event_index = 4
mwifiex_sdio mmc1:0001:1: data_sent=0 cmd_sent=1
mwifiex_sdio mmc1:0001:1: ps_mode=1 ps_state=0
DHCPDISCOVER on eth0 to 255.255.255.255 port 67 interval 9
DHCPDISCOVER on mlan0 to 255.255.255.255 port 67 interval 15
DHCPDISCOVER on eth0 to 255.255.255.255 port 67 interval 13

Further looking into the issue,  I have found a patch  for "eSDHC misses SDIO interrupt when CINT is disabled" for imx processors.

https://patchwork.kernel.org/patch/2446091/

Does this patch is applicable to imx6 processors? If yes, do you have a patch for 3.0.35 kernel?

Thanks in advance,

Krishnan.

标签 (2)
33 回复数

14,028 次查看
supriya_1
Contributor I

Hi ,

I want to know if anyone has been able to do wifi-direct on iMX6 with wfd0 interface if so plz share the steps.

Thnaks

0 项奖励
回复

14,040 次查看
krishnanp
Contributor III

Any pointers in this issue. Appreciate your help...

0 项奖励
回复

14,040 次查看
varsmolta
Contributor V

According to the /drivers/mmc/host/sdhci-esdhc-imx.c file in the imx6Q kernel, this patch should not be applied since that problem should not occur in i.mx6. Look here:

linux-imx6/drivers/mmc/host/sdhci-esdhc-imx.c at boundary-imx_3.0.35_4.0.0 · boundarydevices/linux-i...

But just to double check, have you tried probing the SDIO DAT1 pin to see if it stays low until the card is reset? If this is the case, then the interrupt is not being serviced.

Also, according to this:

Linux/drivers/net/wireless/mwifiex/fw.h - Linux Cross Reference - Free Electrons

Timeout cmd id (97.892473) = 0xce, corresponds to the command HostCmd_CMD_11N_ADDBA_REQ, which is a Block Acknowledgement request cmd. This is an 802.11n feature (Block acknowledgement - Wikipedia, the free encyclopedia). Its possible that the mwifiex driver you are could be out of date. It is at least 2 yrs old according to here:linux-imx6/drivers/net/wireless/mwifiex at boundary-imx_3.0.35_4.0.0 · boundarydevices/linux-imx6 · .... So would suggest updating this to a later version from the mainline linux kernel. You may not be able to do this because of other incompatibilities with the 3.0.35 kernel. So another approach is to load the 3.9 kernel for the sabrelite by following these instructions:i.MX6x SABRE Lite - Linux on ARM - eewiki and seeing if the problem persists.


Also, there is an updated firmware file for the 8787 chipset. Have you given this a try?: kernel/git/firmware/linux-firmware.git - Repository of firmware blobs for use with the Linux kernel. My guess is this fimrware will work with the latest 3.9 kernel.

0 项奖励
回复

14,040 次查看
varsmolta
Contributor V

Also to glean some more info (from here:RE: [PROBLEM] linux-3.2.7:mwifiex:when associating with ap ,there are some strange warning (Linux Wi...):

In kernel .config file (or through menuconfig):

CONFIG_DYNAMIC_DEBUG=y

Re-compile the whole kernel tree, install and reboot. Before running wpa_supplicant, turn on debug:

mkdir /tmp/debug

mount -t debugfs debugfs /tmp/debug

echo "module mwifiex +p" > /tmp/debug/dynamic_debug/control

echo "module mwifiex_sdio +p" > /tmp/debug/dynamic_debug/control

cat /tmp/debug/mwifiex/mlan0/info

After command timeout happens,

cat /tmp/debug/mwifiex/mlan0/debug

Here is some debug info that the driver spits out: Linux/drivers/net/wireless/mwifiex/README - Linux Cross Reference - Free Electrons

0 项奖励
回复

14,040 次查看
krishnanp
Contributor III

Hello varsmolta,

Thank you for the help.

The SDIO DAT1 line has been probed and that is toggling so  we can rule out the interrupt related patch. I have enabled the debug option in kernel and

captured the debug info pls see the logs below.

Bringing up the new kernel may take some time so I kept that option to last one to try.

Meanwhile I have tried another sdio based wifi module on the board. This driver also giving same kind of issue.

The  Wi-Fi driver was working with a different arm platform.  This lead me  to suspect sdio driver in host. What are the issues identified with sdio driver for i.MX6 ?

Did any one used SDIO based wifi module on an  i.MX6 platform?

I want to close this doubt before switching to higher version of kernel..

Appreciate your help.

------------------

Logs

-------------------

After the association with AP

-----------------------------

root@freescale ~$ cat /tmp/debug/mwifiex/mlan0/info

driver_name = "mwifiex"

driver_version = mwifiex 1.0 (14.66.9.p96)

verext = w8787-Ax, RF878X, FP66, 14.66.9.p96, BT_SDIO

interface_name="mlan0"

bss_mode="Ad-hoc"

media_state="Connected"

mac_address="4c:aa:16:c2:0f:ca"

multicast_count="1"

essid="dlink"

bssid="1c:7e:e5:58:77:2b"

channel="6"

region_code = "10"

multicast_address[0]="01:00:5e:00:00:01"

num_tx_bytes = 0

num_rx_bytes = 0

num_tx_pkts = 0

num_rx_pkts = 0

num_tx_pkts_dropped = 0

num_rx_pkts_dropped = 0

num_tx_pkts_err = 0

num_rx_pkts_err = 0

carrier on

tx queue started

root@freescale ~$ cat /tmp/debug/mwifiex/mlan0/info

driver_name = "mwifiex"

driver_version = mwifiex 1.0 (14.66.9.p96)

verext = w8787-Ax, RF878X, FP66, 14.66.9.p96, BT_SDIO

interface_name="mlan0"

bss_mode="Ad-hoc"

media_state="Connected"

mac_address="4c:aa:16:c2:0f:ca"

multicast_count="1"

essid="dlink"

bssid="1c:7e:e5:58:77:2b"

channel="6"

region_code = "10"

multicast_address[0]="01:00:5e:00:00:01"

num_tx_bytes = 0

num_rx_bytes = 0

num_tx_pkts = 0

num_rx_pkts = 0

num_tx_pkts_dropped = 0

num_rx_pkts_dropped = 0

num_tx_pkts_err = 0

num_rx_pkts_err = 0

carrier on

tx queue started

root@freescale ~$ cat /tmp/debug/mwifiex/mlan0/debug

int_counter=0x0

wmm_ac_vo=0x0

wmm_ac_vi=0x0

wmm_ac_be=0x0

wmm_ac_bk=0x0

max_tx_buf_size=0x800

tx_buf_size=0x700

curr_tx_buf_size=0x0

ps_mode=0x1

ps_state=0x3

is_deep_sleep=0x1

wakeup_dev_req=0x1

wakeup_tries=0x0

hs_configured=0x0

hs_activated=0x0

num_tx_timeout=0x0

num_cmd_timeout=0x0

timeout_cmd_id=0x0

timeout_cmd_act=0x0

last_cmd_id=0x6 0x12 0xe4 0x71 0x28

last_cmd_act=0x3 0x7e1c 0xff 0x0 0x113

last_cmd_index=0x3

last_cmd_resp_id=0x8006 0x8012 0x80e4 0x8071 0x8028

last_cmd_resp_index=0x3

last_event=0x17 0x2b 0xa 0xb 0xa

last_event_index=0x3

num_cmd_h2c_fail=0x0

num_cmd_sleep_cfm_fail=0x0

num_tx_h2c_fail=0x0

num_evt_deauth=0x0

num_evt_disassoc=0x0

num_evt_link_lost=0x0

num_cmd_deauth=0x0

num_cmd_assoc_ok=0x1

num_cmd_assoc_fail=0x0

cmd_sent=0x0

data_sent=0x0

cmd_resp_received=0x0

event_received=0x0

cmd_pending=0x0

tx_pending=0x0

rx_pending=0x0

root@freescale ~$ cat /tmp/debug/mwifiex/mlan0/debug

int_counter=0x0

wmm_ac_vo=0x0

wmm_ac_vi=0x0

wmm_ac_be=0x0

wmm_ac_bk=0x0

max_tx_buf_size=0x800

tx_buf_size=0x700

curr_tx_buf_size=0x0

ps_mode=0x1

ps_state=0x3

is_deep_sleep=0x1

wakeup_dev_req=0x1

wakeup_tries=0x0

hs_configured=0x0

hs_activated=0x0

num_tx_timeout=0x0

num_cmd_timeout=0x0

timeout_cmd_id=0x0

timeout_cmd_act=0x0

last_cmd_id=0x6 0x12 0xe4 0x71 0x28

last_cmd_act=0x3 0x7e1c 0xff 0x0 0x113

last_cmd_index=0x3

last_cmd_resp_id=0x8006 0x8012 0x80e4 0x8071 0x8028

last_cmd_resp_index=0x3

last_event=0x17 0x2b 0xa 0xb 0xb

last_event_index=0x4

num_cmd_h2c_fail=0x0

num_cmd_sleep_cfm_fail=0x0

num_tx_h2c_fail=0x0

num_evt_deauth=0x0

num_evt_disassoc=0x0

num_evt_link_lost=0x0

num_cmd_deauth=0x0

num_cmd_assoc_ok=0x1

num_cmd_assoc_fail=0x0

cmd_sent=0x0

data_sent=0x0

cmd_resp_received=0x0

event_received=0x0

cmd_pending=0x0

tx_pending=0x0

rx_pending=0x0

After the ping command

-------------------------

root@freescale ~$ cat /tmp/debug/mwifiex/mlan0/debug

int_counter=0x0

wmm_ac_vo=0x0

wmm_ac_vi=0x0

wmm_ac_be=0x0

wmm_ac_bk=0xf

max_tx_buf_size=0x800

tx_buf_size=0x700

curr_tx_buf_size=0x0

ps_mode=0x1

ps_state=0x0

is_deep_sleep=0x1

wakeup_dev_req=0x0

wakeup_tries=0x0

hs_configured=0x0

hs_activated=0x0

num_tx_timeout=0x0

num_cmd_timeout=0x1

timeout_cmd_id=0xce

timeout_cmd_act=0x1c00

last_cmd_id=0x6 0x12 0xe4 0x71 0xce

last_cmd_act=0x3 0x7e1c 0xff 0x0 0x1c00

last_cmd_index=0x4

last_cmd_resp_id=0x8006 0x8012 0x80e4 0x8071 0x8028

last_cmd_resp_index=0x3

last_event=0xb 0xb 0xb 0xb 0xa

last_event_index=0x4

num_cmd_h2c_fail=0x0

num_cmd_sleep_cfm_fail=0x0

num_tx_h2c_fail=0x0

num_evt_deauth=0x0

num_evt_disassoc=0x0

num_evt_link_lost=0x0

num_cmd_deauth=0x0

num_cmd_assoc_ok=0x1

num_cmd_assoc_fail=0x0

cmd_sent=0x1

data_sent=0x1

cmd_resp_received=0x0

event_received=0x0

cmd_pending=0x0

tx_pending=0x21

rx_pending=0x0

Tx BA stream table:

tid = 0, ra = 1c:7e:e5:58:7

0 项奖励
回复

14,040 次查看
raymondwang
Senior Contributor I

I tried with AzureWare NH-387 module which is also Marvell SD8787 based wireless module on iMX6 sabresd board.

It does work.Fortunately I got marvell newer driver 14.66.35.p16. Both sta and uap work on iMX6 android platform.

0 项奖励
回复

14,028 次查看
brackzhang
Contributor I

hi Raymond Wang:

I will move SD8787 to imx6dq(kernel 3.10.53,android 5.0),following your suggestion, I found some fucntion doest'n match,can you give me how to midify it,looking forward your help

0 项奖励
回复

14,040 次查看
krishnanp
Contributor III

Hi varsmolta & raymond

Thanks a bunch for your help.

I have taken mwifiex driver in 3.2.39 kernel to 3.0.35 kernel and now device working fine in Adapter mode. This proves that no issue on processor interface side.

Now I need to enable uAP support on 3.0.35?

I have checked out 3.10 kernel and analyzed the changes  with 3.0.35. Looks like a lot of changes happened in mainline.

Can you suggest a starting point where I can start down porting ? A of list of changes will help me...

0 项奖励
回复

14,039 次查看
raymondwang
Senior Contributor I

I'd like to share my driver porting on iMX6 android 4.2.2 with you.

1. my wireless relevant code on BoardConfig.mk:

TARGET_KERNEL_MODULES := \

    kernel_imx/net/wireless/cfg80211.ko:system/lib/modules/cfg80211.ko

BOARD_WPA_SUPPLICANT_DRIVER := NL80211

WPA_SUPPLICANT_VERSION := VER_0_8_X

BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_mrvl8787

BOARD_HOSTAPD_DRIVER := NL80211

BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_mrvl8787

BOARD_WLAN_DEVICE := mrvl8787

BOARD_WLAN_VENDOR := MRVL

WIFI_SDIO_IF_DRIVER_MODULE_PATH  := "/system/lib/modules/mlan.ko"

WIFI_SDIO_IF_DRIVER_MODULE_NAME  := "mlan"

WIFI_SDIO_IF_DRIVER_MODULE_ARG   := ""

WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/sd8xxx.ko"

WIFI_DRIVER_MODULE_NAME := "sd8xxx"

WIFI_DRIVER_MODULE_ARG  := "drv_mode=5 cfg80211_wext=0xc sta_name=wlan uap_name=wlan wfd_name=p2p max_uap_bss=1 fw_name=mrvl/sd8787_uapsta.bin"

WIFI_DRIVER_FW_PATH_PARAM := "/proc/mwlan/config"

WIFI_DRIVER_FW_PATH_STA := "drv_mode=5"

WIFI_DRIVER_FW_PATH_AP :=  "drv_mode=6"

WIFI_DRIVER_FW_PATH_P2P := "drv_mode=5"

2. Attached files:

wifi.zip->/hardware/libhardware_legacy/wifi

marvell.zip->/hardware/imx/wlan

You should note that I just write different drv_mode to sd8xxx.ko driver to change different sta/uap/p2p mode. Details in wlan_src/readme_mlan:

The bit settings of drv_mode are,

  Bit 0 :  STA

  Bit 1 :  uAP

  Bit 2 :  WIFIDIRECT

3.Add a framework overlay file on product makefile

  /frameworks/overlay/core/res/res/values/config.xml

Edit that option:

<!-- List of regexpressions describing the interface (if any) that represent tetherable

         Wifi interfaces.  If the device doesn't want to support tethering over Wifi this

         should be empty.  An example would be "softap.*" -->

    <string-array translatable="false" name="config_tether_wifi_regexs">

      <item>"wlan.*"</item>

    </string-array>

   Note that bolded "wlan.*" match my wlan interface name "uap_name=wlan" (BoardConfig.mk). Since Android does not support WiFi station and uAP mode simultaneously, It does not matter we have the same interface name for station and uAp (sta_name=wlan uap_name=wlan).

  Hope these material can help you!

14,027 次查看
andreygelman
Contributor III

Hello, Raymond !

Thanks for sharing your experience - it helped me a lot in my attempts to configure Wi-Fi on my device.

Now I cannot bring up the hotspot mode ...

After configuring everything more or less the way you suggest, that's what I get in the logcat:

...

D/hostapd ( 3307): nl80211: Register frame type=0x40 nl_handle=0x4054b230

D/hostapd ( 3307): nl80211: Register frame match - hexdump(len=0): [NULL]

D/hostapd ( 3307): nl80211: Register beacons command failed: ret=-95 (Operation not supported on transport endpoint)

E/hostapd ( 3307): nl80211: Failed to set interface wlan0 into AP mode

D/hostapd ( 3307): netlink: Operstate: linkmode=0, operstate=6

D/hostapd ( 3307): nl80211: Set mode ifindex 9 iftype 2 (STATION)

E/hostapd ( 3307): nl80211 driver initialization failed.

...

While the hotspot never seems ready, the wlan0 interface does acquire IP address.

Did the hotspot mode work for you ?

What is your hostapd.conf file ?

Are there specific requirements about network capabilities, in order to be able to serve as an hotspot (my device has Ethernet along with Wi-Fi) ?

My system consists of i.MX6, sd8787 (Azurewave), Wi-Fi driver and wpa_supplicant extensions that you have posted above.

Any advice will be highly appreciated !

0 项奖励
回复

14,027 次查看
raymondwang
Senior Contributor I

Please check your wlan driver makefile, enable CONFIG_ANDROID_KERNEL=y (default n).

0 项奖励
回复

14,027 次查看
andreygelman
Contributor III

Cool !

Thank you !

0 项奖励
回复

14,027 次查看
adamlee
Contributor I

Raymond, thank you very much for sharing. It's invaluable!

With wifi up and running, did you get BT working? It's my next goal.

0 项奖励
回复

14,027 次查看
raymondwang
Senior Contributor I

Can you start another thread for sd8787 bluetooth? I am facing same problem about bluetooth stability.

0 项奖励
回复

14,027 次查看
adamlee
Contributor I
0 项奖励
回复

14,027 次查看
adamlee
Contributor I

Sure thing Raymond, I will create one tonight (in 4~5 hours).

Let's do this!

Adam

0 项奖励
回复

14,039 次查看
soursunny
Contributor II

there are something wrong....??

make: *** No rule to make target `out/target/product/sabresd_6dq/obj/STATIC_LIBRARIES/lib_driver_cmd_mrvl8787_intermediates/export_includes', needed by `out/target/product/sabresd_6dq/obj/EXECUTABLES/hostapd_intermediates/import_includes'.  Stop.

0 项奖励
回复

14,039 次查看
raymondwang
Senior Contributor I

marvell\wpa_supplicant_8_lib

The private static library is located at marvell\wpa_supplicant_8_lib

you can compile it manually or Add it's Android.mk to your whole building tree.

0 项奖励
回复

14,039 次查看
soursunny
Contributor II

i dont' know how to add it.

it seems that Boardconfig.mk has

WPA_SUPPLICANT_VERSION := VER_0_8_X

and wpa_supplicant_8_lib\android.mk

LOCAL_PATH := $(call my-dir)

ifeq ($(WPA_SUPPLICANT_VERSION),VER_0_8_X)

why can't it compile automatic ?

0 项奖励
回复

14,039 次查看
raymondwang
Senior Contributor I

You can refer to broadcom library in hardware/broadcom/wlan/bcmdhd/wpa_supplicant_8_lib

0 项奖励
回复