SDHCI trap with register dump dropping SDIO clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHCI trap with register dump dropping SDIO clock

9,199 Views
vikramramanna
Contributor I

iMX8MM dropping SDIO clock to 12MHz causes the SDHCI crash

[  641.123790] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[  641.130232] mmc0: sdhci: Sys addr:  0x54968d04 | Version:  0x00000002
[  641.136671] mmc0: sdhci: Blk size:  0x00000004 | Blk cnt:  0x00000001
[  641.143110] mmc0: sdhci: Argument:  0x15804004 | Trn mode: 0x00000013
[  641.149548] mmc0: sdhci: Present:   0x01d88a0a | Host ctl: 0x00000013
[  641.155986] mmc0: sdhci: Power:     0x00000002 | Blk gap:  0x00000080
[  641.162425] mmc0: sdhci: Wake-up:   0x00000008 | Clock:    0x0000028f
[  641.168863] mmc0: sdhci: Timeout:   0x0000008f | Int stat: 0x00000000
[  641.175301] mmc0: sdhci: Int enab:  0x107f100b | Sig enab: 0x107f100b
[  641.181739] mmc0: sdhci: AC12 err:  0x00000000 | Slot int: 0x00000502
[  641.188178] mmc0: sdhci: Caps:      0x07eb0000 | Caps_1:   0x8000b407
[  641.194616] mmc0: sdhci: Cmd:       0x0000353a | Max curr: 0x00ffffff
[  641.201054] mmc0: sdhci: Resp[0]:   0x00001000 | Resp[1]:  0x00000000
[  641.207492] mmc0: sdhci: Resp[2]:   0x00000000 | Resp[3]:  0x00000000
[  641.213930] mmc0: sdhci: Host ctl2: 0x00000088
[  641.218372] mmc0: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x5608d208
[  641.224809] mmc0: sdhci: ============================================

NXP team, can someone point to what could be the reason

Don't see any issue with iMX8MQ or iMX6/7

0 Kudos
Reply
27 Replies

7,398 Views
ramesh_r
Contributor I

Actually you should see it on both, our recent test was run on imx8mnevk board with L5.4.3 BSP where we saw this issue. So, the problem is reproducible using either of the boards.

Regards

Ramesh

0 Kudos
Reply

7,397 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ramesh,

Could you send us your full log file test on our NXP BSP and board?

From the screenshot customer send, there are errors reported from brcmfmac/sdio.c. So are you using i.MX8MM DDR4 EVK with cyw43455 wifi module, not i.MX8MM LPDDR4 EVK with qca9377 wifi module? Tell us.

Our experts use i.MX8MM DDR4 EVK, Linux 5.4.3_1.0.0 BSP version with cyw43455 wifi module loaded, download from Embedded Linux for i.MX Applications Processors | NXP .  When drop mmc0(sdio) clock from 208MHz to 12MHz using your method, wait for several times, the timeout issue will not happen.  Log is as attached.

So there are some hareware/software differences between us?

Have a nice day

Best Regards

Rita

0 Kudos
Reply

7,395 Views
ramesh_r
Contributor I

Hi Rita,

The last test was run on NXP IMX8MNEVK / DDR4 with a cyw43455-sdio card, using image built from NXP's L5.4.3 BSP. But the test method is different from my earlier method. In this case, a dts entry is added to set the max-frequency for the SDHC interface & the corresponding .dtb file is used during bootup.  Once you bring up the wlan interface up, you should hit the condition. Please find the dmesg log from the test attached. I am also attaching the .dts & .dtb files used in the test.

Regards

Ramesh

0 Kudos
Reply

7,394 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ramesh,

We found that your cyw43455 wifi firmware version (version 7.45.206) is different with NXP offical release(version 7.45.184). So suggest you to use wifi firmware from offical release, namely brcmfmac43455-sdio.bin from imx-firmware/cyw-wifi-bt/1MW_CYW43455 at master · NXP/imx-firmware · GitHub . Also from log, seems you add Murata’s customized layer "meta-murata-wireless" which gets hooked into the i.MX build, are you using the official Linux 5.4.3_1.0.0 BSP download from Embedded Linux for i.MX Applications Processors | NXP ?

 

We need confirm with you that is the 12MHz means SDR12 mode? Is it always happens on your side?

Have a nice day

Best Regards

Rita

0 Kudos
Reply

7,394 Views
ramesh_r
Contributor I

Hi Rita,

With the .dts file that I attached earlier, you don't see the issue ?  I will revert back with answers for your other comments.

Regards

Ramesh

0 Kudos
Reply

7,394 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

We found that your cyw43455 wifi firmware version (version 7.45.206) is different with NXP offical release(version 7.45.184). So suggest you to use wifi firmware from offical release, namely brcmfmac43455-sdio.bin from imx-firmware/cyw-wifi-bt/1MW_CYW43455 at master · NXP/imx-firmware · GitHub . Also from log, seems you add Murata’s customized layer "meta-murata-wireless" which gets hooked into the i.MX build, are you using the official Linux 5.4.3_1.0.0 BSP download from Embedded Linux for i.MX Applications Processors | NXP ?

 

We need confirm with you that is the 12MHz means SDR12 mode? Is it always happens on your side?

0 Kudos
Reply

7,394 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you also send us the log file?

0 Kudos
Reply

7,399 Views
vikramramanna
Contributor I

Reference board i.MX 8M Mini Evaluation Kit | NXP 

Also on this hardware iMX8M Mini uCOM Developer's Kit V2 - Embedded Artists 

Dont see the issue on iMX8M Quad Developer's Kit V2 - Embedded Artists  or other iMX series

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you mean you meet this question in our i.MX8MM EVK board? If yes, I will do confirm it for you.

0 Kudos
Reply

7,399 Views
vikramramanna
Contributor I

Sorry did not understand your question.

The SDHCI crashes, is there any driver update or fix from the crash dump i've provided above ?

Are there any known issues with iMX8MM in particular ?

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell me which version BSP are you using?

0 Kudos
Reply

7,399 Views
vikramramanna
Contributor I

#define SDHCI_HOST_VERSION      0xFE

is from sdhci.c file

also if you see the crash dump 

it says Version 02


Is there some place I can look for ?

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Can you tell us which mode did you configured for the SDHC system? I have sent your question to our expert team. And our expert are confirming it for you.

0 Kudos
Reply

7,399 Views
vikramramanna
Contributor I

Mode is 4bit SDIO mode

Operation freq is 12Mhz.

Can this be treated as priority. Looks like a bug in the driver implementation of SDHC.

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Vikram,

Could you tell us which version BSP are you using? L5.4.3_1.0.0 or L4.19.35_1.1.0 or other version. We need know this for further confirming.

Have a nice day

Rita

0 Kudos
Reply

7,399 Views
vikramramanna
Contributor I

This is the BSP version is 4.14.98-2.2.0

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Vikram,

This is the update from our expert. Hope this can do help for you.

After doing a bit o research I have found in the Release Notes that BSP version 4.14.98-2.2.0  is not GA tested for iMX8MM. My recommendation for the customer is to switch to a GA release such as 4.14.98-2.0.0_ga or newer (4.19.35 or 5.4) and try dropping the SDIO clock to 12MHz on that release.

Have a nice day

Best Regards

Rita

0 Kudos
Reply

7,399 Views
ramesh_r
Contributor I

Hi Rita,

This same test was run on using NXP's L5.4.3 BSP release and the problem is still observed. When the mmc clock is changed to 12Mhz, this message is observed with a dump:

Timeout waiting for hardware interrupt

drivers/mmc/host/sdhci.c:sdhci_timeout_data_timer <== Here is the source & function. Attaching a screenshot for ref.

Can you please help?IMX8MM-12Mhz.jpg

0 Kudos
Reply

7,399 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will confirm it for you.

0 Kudos
Reply

7,399 Views
ramesh_r
Contributor I

Hi Rita,

Just checking to see if you heard anything on this?

Regards

Ramesh

0 Kudos
Reply