SDHC / SDXC Support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,594件の閲覧回数
semihhazar
Contributor II

Hi All,

I checked the reference manual but couldn't see any info regarding SD card support. Does imx28 support SDHC and/or SDXC cards?

Best Regards,

Semih

ラベル(1)
タグ(3)
1 解決策
3,218件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Semih

imx28 supports SDHC but not SDXC cards.

Best regards

chip

元の投稿で解決策を見る

4 返答(返信)
3,219件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Semih

imx28 supports SDHC but not SDXC cards.

Best regards

chip

3,217件の閲覧回数
semihhazar
Contributor II

Thanks for the reply.

BR,

Semih

0 件の賞賛
返信
3,218件の閲覧回数
pt
Senior Contributor I

IMX28 supports sd card. SSP support sd/sdio and mmc

Multimedia Applications Processor|Freescale

Check this section in reference manual 17.8 SD/SDIO/MMC Mode

0 件の賞賛
返信
3,217件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Check the chapter 17 Synchronous Serial Ports (SSP)

The SSP supports MMC/SD/SDIO 1-bit, 4-bit, and 8-bit modes.

Best Regards,

Luis

0 件の賞賛
返信