SDHC / SDXC Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHC / SDXC Support

Jump to solution
3,621 Views
semihhazar
Contributor II

Hi All,

I checked the reference manual but couldn't see any info regarding SD card support. Does imx28 support SDHC and/or SDXC cards?

Best Regards,

Semih

Labels (1)
Tags (3)
1 Solution
3,245 Views
igorpadykov
NXP Employee
NXP Employee

Hi Semih

imx28 supports SDHC but not SDXC cards.

Best regards

chip

View solution in original post

4 Replies
3,246 Views
igorpadykov
NXP Employee
NXP Employee

Hi Semih

imx28 supports SDHC but not SDXC cards.

Best regards

chip

3,244 Views
semihhazar
Contributor II

Thanks for the reply.

BR,

Semih

0 Kudos
Reply
3,245 Views
pt
Senior Contributor I

IMX28 supports sd card. SSP support sd/sdio and mmc

Multimedia Applications Processor|Freescale

Check this section in reference manual 17.8 SD/SDIO/MMC Mode

0 Kudos
Reply
3,244 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Check the chapter 17 Synchronous Serial Ports (SSP)

The SSP supports MMC/SD/SDIO 1-bit, 4-bit, and 8-bit modes.

Best Regards,

Luis

0 Kudos
Reply