SDHC Class 10 Boot -Processor Part Number?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDHC Class 10 Boot -Processor Part Number?

1,281件の閲覧回数
balajipadmanaba
Contributor I

Can somebody Suggest a Processor which can have a SDHC card has a boot interface?

UART-3

SPI-2

ADC-2.

JTAG

ADC-2

Secondary Boot

SRAM min-512KB

SDHC-Transfer speed 10MB/s should support class 10

----------------

DDR2- if available not manadatory

I see no micro controller doing SDHC boot from my trade study.

But a micro controller is can do all except SDHC boot with boot options to the next boot device no bootstrap is available on it?.

Any help or suggestions of part numbers?

0 件の賞賛
返信
1 返信

1,217件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi balaji

one can check i.MX comparison table

https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信