SCU FW debugging method

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCU FW debugging method

ソリューションへジャンプ
2,976件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

We would like to use the JTAG debugger for SCU FW development.

Is it possible? or should we use debug print via SCU_UART? 

<Target Environment>

SoC : i.MX8QuadMax

Best Regards,

Kazuma Sasaki.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,900件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

for SCFW debugging one can refer to AN12631 sect.3.2 SCFW Debugging

Normal and Secure Debug for i.MX8/8X Family of Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,900件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

for SCFW debugging one can refer to AN12631 sect.3.2 SCFW Debugging

Normal and Secure Debug for i.MX8/8X Family of Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,900件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your support. I confirmed that jtag debug is possible at SCFW.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信