SCU FW debugging method

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCU FW debugging method

Jump to solution
2,976 Views
Kazuma_Sasaki
Senior Contributor I

We would like to use the JTAG debugger for SCU FW development.

Is it possible? or should we use debug print via SCU_UART? 

<Target Environment>

SoC : i.MX8QuadMax

Best Regards,

Kazuma Sasaki.

Tags (1)
0 Kudos
Reply
1 Solution
2,900 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

for SCFW debugging one can refer to AN12631 sect.3.2 SCFW Debugging

Normal and Secure Debug for i.MX8/8X Family of Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,900 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

for SCFW debugging one can refer to AN12631 sect.3.2 SCFW Debugging

Normal and Secure Debug for i.MX8/8X Family of Applications Processors

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,900 Views
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your support. I confirmed that jtag debug is possible at SCFW.

Best Regards,

Kazuma Sasaki.

0 Kudos
Reply