SCFW: how to use RPC protocol to get a resource access from Linux, to use a hw peripheral

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCFW: how to use RPC protocol to get a resource access from Linux, to use a hw peripheral

4,265 Views
dry
Senior Contributor I

Anyone can provide a detailed code example of how to use this RPC protocol, to communicate from the Ax cores/Linux to SCFW or the cores that own a resource I want, to get access to that resource...?

Can I do / use The Resource Management (RM) API"  this way, through RPC ..?

Does this only work at kernel level, and then needs a user-space client, like scfw_cli app...?

I don't understand how scfw_cli app works, can it invoke Any of those SCFW APi calls ..? Can it do the RM stuff...?  Example please ..??

 

Tags (1)
0 Kudos
Reply
6 Replies

2,092 Views
flobro
Contributor IV
0 Kudos
Reply

2,092 Views
flobro
Contributor IV

Posting links to the SCFW porting guide is not a reasonable answer to the questions. At least tell people that there is currently NO solution to user space SCFW register access unless YOU write a device driver yourself (and the user space app that uses it). I would love to read the pad/mux register to verify the settings, but no such luck.

I have read the porting guide and it is not helpful to someone who wants to possibly write a driver to set/get values for development mode.

0 Kudos
Reply

4,137 Views
13614278
Contributor III

Yeah, no offensive, but I have to say, it is really pity that the document is too poor for this scfw api.

It seems there are so many pdf/html, but just a full list plain text, without any useful info 

0 Kudos
Reply

4,242 Views
jimmychan
NXP TechSupport
NXP TechSupport

You could download the SCFW porting kit from here. There is source code and the documentation in the porting kit.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

e.g. SCFW Porting Kit​ 1.14.0

0 Kudos
Reply

4,236 Views
dry
Senior Contributor I

@jimmychan 

Yes, I got it, and seems you have to modify Linux kernel to allow user-space app to use the SC services ...

Also no clear example how to, for example, ask resource owner to use it from another domain .?

0 Kudos
Reply

4,227 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply