SCFW change memory map

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCFW change memory map

1,432件の閲覧回数
xu_ji1
Contributor V

Hi,

Now we used 512MB DDR on i.MX8X platform,and I need to change the memory map in code

How to set below code about 512MB memory?

/* Board has 3GB memory so fragment upper region and retain 1GB */
BRD_ERR(rm_memreg_frag(pt_boot, &mr_temp, 0x8C0000000ULL,
0xFFFFFFFFFULL));

/* Move M4 0 TCM */
BRD_ERR(rm_find_memreg(pt_boot, &mr_m4_0, 0x034FE0000ULL,
0x034FE0000ULL));
BRD_ERR(rm_assign_memreg(pt_boot, pt_m4_0, mr_m4_0));

/* Reserve DDR for M4_0 */
BRD_ERR(rm_memreg_frag(pt_boot, &mr_m4_0,
0x088000000ULL, 0x08FFFFFFFULL));
BRD_ERR(rm_assign_memreg(pt_boot, pt_m4_0, mr_m4_0));

/* Reserve FlexSPI for M4_0 */
BRD_ERR(rm_memreg_frag(pt_boot, &mr_m4_0, 0x08081000ULL,
0x08180FFFULL));

/* Create shared memory space */
BRD_ERR(rm_memreg_frag(pt_boot, &mr_sh,
0x090000000ULL, 0x091FFFFFFULL));

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,421件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xu

 

additional patches were sent via mail, also may be useful:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8X-5-4-24-kernel-customization-appli...

 

Best regards
igor

0 件の賞賛
返信