SATA performance degradation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SATA performance degradation

2,521 Views
myungjukim
Contributor II

Hi, Community

I've update kernel 3.14.28 to 3.14.52 recently. I've connect hdd(2T) to sata interface.

but I've found performance degradation regardless which format have with sata hdd read/write test.

Result is HUGE degradation between 3.14.28 and 3.14.52. How to remove SATA degradation point ?

<test>

file system is based on ext4. bsp is commercial.

cpu : imx6dual

command : iozone -a -n 4096m -g 4096m -i 0 -i 1 -f /mnt/HDD1/iozone.tmpfile -Rb ./iozone

<test result>

- 3.14.28 kernel : write 100Mb/s, read 120Mb/s

- 3.14.52 kernel : write15Mb/s, read 60Mb/s

Labels (4)
0 Kudos
Reply
3 Replies

2,305 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian 

could you try nxp L3.14.52 bsp

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/mach-imx?h=imx_3.14.52_1.1...

for non-nxp bsps one can post on  meta-fsl-arm mailing list, so that someone familiar with

it could try to assist you

meta-freescale Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,305 Views
myungjukim
Contributor II

Hi, igor

I'm using nxp official bsp on your  document. I think correct download bsp.

         Freescale Yocto Project User's Guide, Rev. 0, 12/2015 , page 13

         repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga

I think, It is not file system issue. It is lower access speed to the SATA controller integrated into the main CPU/SoC.

I've download your 4.1.15 bsp and test it. It's speed  is write 12.5 MB/s and read 42 MB/s .

I get same result on your reference board(imx6q_sabresd).

Best Regards

0 Kudos
Reply

2,305 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian 

please check

https://community.nxp.com/message/859275

Best regards
igor

0 Kudos
Reply