How do I implement spread spectrum on iMX6Dual in Yocto 3.10?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I implement spread spectrum on iMX6Dual in Yocto 3.10?

1,001 Views
davesimonson
Contributor I

I have seen the document that describes flash_headr.S, but that isn't part of Yocto.

I tried to add the code from that document into lowlevel_init.S

The result simply fails to boot.

Labels (2)
0 Kudos
Reply
1 Reply

836 Views
igorpadykov
NXP Employee
NXP Employee

Hi DAVE

please check

enable the spread spectrum 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply