SATA corruption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SATA corruption

3,843件の閲覧回数
karanbhagoji
Contributor II

Hello all,

We have custom boards with imx6 quad processor with android jelly bean running on 3.0.35 kernel with SATA boot , size 30 gb .  After using the board for some time we are getting a SATA corruption messages, the errors are different for different boards, like eg

1->

EXT4-fs error (device sda4): ext4_lookup:1044: inode #22: comm er.ServerThread: deleted inode referenced: 69

Aborting journal on device sda4-8.

Kernel panic - not syncing: EXT4-fs (device sda4): panic forced after error

CPU0: stopping

[<c0131f84>] (unwind_backtrace+0x0/0x138) from [<c01243a8>] (do_IPI+0x1d4/0x208)

2->

ata1.00: exception Emask 0x1 SAct 0x1f SErr 0x0 action 0x6 frozen

ata1.00: irq_stat 0x40000000

ata1.00: cmd 60/08:00:00:90:84/00:00:02:00:00/40 tag 0 ncq 4096 in

         res 40/00:18:60:e5:80/00:00:02:00:00/40 Emask 0x1 (device error)

3->

DVFS driver module loaded

rtc-m41t80 0-0068: setting system clock to 2055-09-11 10:21:10 UTC (2704270870)

Freeing init memory: 1136K

4->

binder: 4716:4716 transaction failed 29189, size 80-4

binder: 4716:4716 transaction failed 29189, size 212-4

We getting stuck in this error. Due to these errors the displays hangs at splash screen with no android UI prompt .All the errors indicate that the SATA cards are getting corrupted. Is there any error with the JB android /  kernel/ anything  which is causing this corruption?

Kindly advice , also suggest solutions if any.

Regards,

Karan

4 返答(返信)

3,520件の閲覧回数
karanbhagoji
Contributor II

Hello Ambika ,

Sorry for the late reply , but the above  suggestion is  true , it is due to improper power supply and etc. Abrupt power off after long time is the main reason as the journalling is not updated, and hence may lead to sata corruption, also to add , during power off if the journalling regions are corrupt then there is no way to update the same and hence error. Also recommend to check the connectors for loose connections .

Regards,

Karan

0 件の賞賛
返信

3,520件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Karan

corruption may be caused by sudden turn of power supplies,

recommended to use linux poweroff command.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,520件の閲覧回数
karanbhagoji
Contributor II

Hello Igor,

Agreed that the sudden turn turn off of power supplies may be  an issue here, but its not always the case, the device boots

after an abrupt power supply failure I have already tried to turn off the power supply abruptly many times, but the SATA card is not getting corrupted..

Please suggest any way to overcome this corruption.

Regards,

Karan

0 件の賞賛
返信

3,520件の閲覧回数
ambika
Contributor II

Hi Karan,

I have the same problem of firmware getting corrupted with sata boot in imx6q board, whether have you got any clues??

Thanks & Regards,

Ambika

0 件の賞賛
返信