SAI3 port data line's pull select fields

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAI3 port data line's pull select fields

1,012 Views
ganapathiraopil
Contributor I

Hi,

I am trying to add a new sound card as an external mic to record the voice in imx7d board, for this I am configuring sai3 port. For sai3 , the available pull select fields are 100K PD, 5K PU, 47K PU and 100K PU. So on which basis we need to select these values. Do we have any proper format to follow while configuring these pull fields or we can have any of these available values?.

Kernel version - 4.1.15

Please help me regarding this.

Thanks in advance.

Regards,

Ganapathirao

Labels (1)
0 Kudos
Reply
1 Reply

935 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganapathirao

some signals may be tristated (both codec and i.MX7) as described in

Table 13-44. SAI External Signals i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

so pad settings should be set appropriately. Settings provided in NXP

software : linux and FreeRTOS bsps can be used as starting point

and adjusted based on waveforms required by datasheet.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply