[SABRESD/Android 4.4] USB speakerphone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[SABRESD/Android 4.4] USB speakerphone

1,719件の閲覧回数
norisugi
Contributor II

I tried the usb speakerphone.

The mic input is OK, but the speaker output is NG.

The sound is output from HDMI side.

Does anyone have any idea to solve this issue ?

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,570件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Nori,

The attached patches are based on kk4.4.2_1.0.0-ga_rc3

Please apply imx-usbheadset under hardware/imx and fsl-usbheadset under device/fsl


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,570件の閲覧回数
norisugi
Contributor II

Hi Sergio-san,

Thank you for your patch.

But this patch is not perfect.

USB mic is recognized as USB audio device which has both in and out .

So the sound is not output from HDMI.

Do  you have any idea about this issue ?

Best Regards,

Nori

0 件の賞賛
返信