[SABRESD/Android 4.4] USB speakerphone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[SABRESD/Android 4.4] USB speakerphone

1,296 Views
norisugi
Contributor II

I tried the usb speakerphone.

The mic input is OK, but the speaker output is NG.

The sound is output from HDMI side.

Does anyone have any idea to solve this issue ?

Labels (2)
0 Kudos
Reply
2 Replies

1,147 Views
SergioSolis
NXP Employee
NXP Employee

Hello Nori,

The attached patches are based on kk4.4.2_1.0.0-ga_rc3

Please apply imx-usbheadset under hardware/imx and fsl-usbheadset under device/fsl


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,147 Views
norisugi
Contributor II

Hi Sergio-san,

Thank you for your patch.

But this patch is not perfect.

USB mic is recognized as USB audio device which has both in and out .

So the sound is not output from HDMI.

Do  you have any idea about this issue ?

Best Regards,

Nori

0 Kudos
Reply