SABRE iMX53 WinCE7 camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE iMX53 WinCE7 camera

1,995 Views
rajeshg
Contributor I

Hi I am trying to get the camera output into the encoder (VPU). And I am having a few issues, can you please help me with these?

1. CSPROPERTY_TYPE_GET on CSPROPERTY_CONNECTION_ALLOCATORFRAMING returns 1 for RequirementsFlags which means that the driver will allocate and maintain the buffers. Is there a way to have client control the buffers? I see iMX27 implementation supports IOCTL_SET_DIRECT_CAPTURE_MODE command. which is not available in Camera.h for iMX53.

2. When I try to read the data ranges for all the pins (PREVIEW, CAPTURE and STILL) the following are the formats supported for each pin

          PREVIEW - RGB and YV12

          CAPTURE - UYVY

          STILL - RGB

But the document says Capture supports UYVY, YV12 and NV12, but thats not what is returned.

I dont see NV12 for any pin.

Can you please help me with these two issues?

Also, Is there a documentation on Camera APIs and VPU APIs ?

Thanks

Rajesh

Labels (3)
0 Kudos
Reply
3 Replies

1,815 Views
YixingKong
Senior Contributor IV

Rajesh

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

1,815 Views
YixingKong
Senior Contributor IV

Rajesh

We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,815 Views
YixingKong
Senior Contributor IV

Rajesh

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 Kudos
Reply