SABRE SD BARD SPI NOR bootup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE SD BARD SPI NOR bootup

1,303件の閲覧回数
jamesdavis
Contributor III

Hi,

It looks like the i.MX6 SABRE-SD cannot boot from SPI NOR flash. See the highlighted known issue below, which comes from i.MX6 Linux release note.

However, the i.MX6 SABRE-AI board can boot from SPI NOR. It uses EIM_D16/17/18/19 pins.

Is there a way to use other ECSPI ports to support bootup by i.MX6 ROM bootstrap?

i.MX6 SABRE-SD Known Issues.jpg

Thanks,

James

ラベル(1)
0 件の賞賛
返信
1 返信

1,240件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi James

Table 8-25. SPI IOMUX Pin Configuration IMX6DQRM

shows other available options for boot from ecspi.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信