SABRE SD BARD SPI NOR bootup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SABRE SD BARD SPI NOR bootup

1,304 次查看
jamesdavis
Contributor III

Hi,

It looks like the i.MX6 SABRE-SD cannot boot from SPI NOR flash. See the highlighted known issue below, which comes from i.MX6 Linux release note.

However, the i.MX6 SABRE-AI board can boot from SPI NOR. It uses EIM_D16/17/18/19 pins.

Is there a way to use other ECSPI ports to support bootup by i.MX6 ROM bootstrap?

i.MX6 SABRE-SD Known Issues.jpg

Thanks,

James

标签 (1)
0 项奖励
回复
1 回复

1,241 次查看
igorpadykov
NXP Employee
NXP Employee

Hi James

Table 8-25. SPI IOMUX Pin Configuration IMX6DQRM

shows other available options for boot from ecspi.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复