SABRE MX6DQ Android access CAN data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE MX6DQ Android access CAN data

2,007 Views
arun3
Contributor I

SABRE-MX6DQ - Access CAN on Android

Hello 

I have an IMX6 based Android Tablet . This device also has an inbuilt CAN communication chip. However the OEM is not very responsive about documenatation. 

I am trying to access the data from the CAN interface through the Android application. Can you please guide me to theright way to start working on the project. Right now I am fairly lost. Could not get the right mfgtools 

Labels (3)
0 Kudos
Reply
2 Replies

1,962 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

one can try guidelines provided on :

i.MX6q sabresd CAN/FLEXCAN Support 

https://community.nxp.com/thread/307066 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,962 Views
arun3
Contributor I

Thank you Igor. Will check this out and keep you posted. Appreciate the response

0 Kudos
Reply