Boot2QT for i.mx8M Nano

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot2QT for i.mx8M Nano

2,408件の閲覧回数
muha2metaydin
Contributor I

How can i make ready my imx8m Nano device for device creation in other word boot to qt? I examined yocto project documents, qt documents and imx8 documents but i didn't understand. Anyhow i don't even know if it's possible. I built yocto project for my imx8m Nano device however i have no idea about boot2qt part. Does anyone have experience in this regard?

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

2,351件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Muhammet Aydın,

The latest BSP Release (L5.4.3_1.0.0) supports the i.MX8M Nano and there is an image based in Qt5 available. This is the only supported Qt iteration on the BSP.

It is my understanding that Boot2QT was rebranded as Qt for Device Creation.

https://doc.qt.io/QtForDeviceCreation/

You would need to port it to your desired board. However, there are some third party boards from Boundary Devices that do support this stack:

https://doc.qt.io/QtForDeviceCreation/qtdc-supported-platforms.html

I hope this information helps!

Regards,

0 件の賞賛
返信