SABRE Lite powered by USB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Lite powered by USB?

Jump to solution
6,074 Views
patkelly18
Contributor I

I have a SABRE Lite and I was wondering if it was possible to power it via USB rather than the main adapter.

Labels (1)
0 Kudos
Reply
1 Solution
2,630 Views
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

View solution in original post

0 Kudos
Reply
2 Replies
2,631 Views
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

0 Kudos
Reply
2,630 Views
patkelly18
Contributor I

Thanks for the help. I found a work around of sorts. Although it can't be powered through the USB port like a lot of the lower powered boards. I was able to power it via a USB to Type M cable, so use my laptop and the existing power socket and it worked fine.

0 Kudos
Reply