SABRE Lite powered by USB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SABRE Lite powered by USB?

跳至解决方案
6,056 次查看
patkelly18
Contributor I

I have a SABRE Lite and I was wondering if it was possible to power it via USB rather than the main adapter.

标签 (1)
0 项奖励
回复
1 解答
2,612 次查看
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,613 次查看
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

0 项奖励
回复
2,612 次查看
patkelly18
Contributor I

Thanks for the help. I found a work around of sorts. Although it can't be powered through the USB port like a lot of the lower powered boards. I was able to power it via a USB to Type M cable, so use my laptop and the existing power socket and it worked fine.

0 项奖励
回复