SABRE Lite powered by USB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE Lite powered by USB?

ソリューションへジャンプ
6,055件の閲覧回数
patkelly18
Contributor I

I have a SABRE Lite and I was wondering if it was possible to power it via USB rather than the main adapter.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,611件の閲覧回数
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,612件の閲覧回数
the_1080p_guy
Contributor I

The adapter can provide 4A @5V, and as far as i know usb 2.0 only provides 500mA, so i dont think powering from usb is possible... btw,the datasheet says it requires >5W power just to turn on the board without any peripheral

0 件の賞賛
返信
2,611件の閲覧回数
patkelly18
Contributor I

Thanks for the help. I found a work around of sorts. Although it can't be powered through the USB port like a lot of the lower powered boards. I was able to power it via a USB to Type M cable, so use my laptop and the existing power socket and it worked fine.

0 件の賞賛
返信