Running two bin files of M4 same time in ocram and DRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running two bin files of M4 same time in ocram and DRAM

902 Views
narendray
Contributor I

I have two bin files 1.bin and 2.bin   ,first one is compiled to ocram and second one is compiled to Dram i am able to run them seperately,how to run both of them in parallel. 

Labels (1)
0 Kudos
Reply
1 Reply

855 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  It is needed to use multitasking options of Your system.

For FreeRTOS You may look at the following 

RTOS kernel rapidly switches between tasks 

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply